webinar a la carta

Doing Research with Catapult HLS at Harvard

Tiempo estimado de visualización: 29 minutos

Compartir

One of them is about proposing adaptive floating-point (FP) quantization to replace integer (INT) quantization for NNs.

This presentation introduces Harvard's experiences of using Catapult HLS in research projects. Since 2018, we have taped out several chips with hardware components designed in SystemC. The HLS design flow has been very helpful to shorten development cycle of accelerators as well as providing a way to quickly prototype different research ideas. First half of the talk focuses on our learnings with the HLS tool. Even though comparing with Verilog RTL, SystemC allows us to design hardware in a more concise and efficient manner, we find it difficult at first to figure out what kind of coding is more appropriate. Specifically, how to pass HLS and achieve pipeline initial interval “II = 1” for critical parts of accelerator designs. Throughout many trial and errors, we have developed intuitions and strategies for SystemC coding. In addition, we also extensively leverage standard hardware IPs provided in Mentor Algorithmic C and NVIDIA MatchLib to implement our designs. For the second half, we share some projects involving Catapult HLS. One of them is about proposing adaptive floating-point (FP) quantization to replace integer (INT) quantization for NNs, especially for large-scale NLP models. For hardware evaluation of this idea, we utilize Catapult HLS and PowerPro to compare power and area of FP and INT MAC datapath designs. The work has been selected as the best research paper in DAC 2020 conference.

Conoce al invitado

Harvard University

En-Yu Daniel Yang

PhD Student

En-Yu (Daniel) Yang is a PhD student in Computer Science at Harvard. He received B.S. in Electrical Engineering from National Tsing Hua University in 2018. His research focuses on specialized architecture and hardware design for machine learning applications. He has been working on designing accelerators using SystemC with Catapult HLS tool, and some of his work is accepted in DAC’20 and ISSCC’21 conferences.

Recursos relacionados

Xperi®: A Designer’s Life with HLS
Webinar

Xperi®: A Designer’s Life with HLS

This webinar will discuss two aspects of their experience going from RTL to HLS. The first topic is using HLS for algorithms such as Face Detection th

High-Level Synthesis Verification Technologies and Techniques
Webinar

High-Level Synthesis Verification Technologies and Techniques

This session will describe applying known and trusted static, formal and dynamic approaches to verification performed at the C++ or SystemC HLS level of abstraction.

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques
Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations.