seminario web a la carta

Efficient aircraft certification

Avoid issues that delay aircraft certification.

Tiempo estimado de visualización: 60 minutos

Compartir

An airplane flies up and to the right with clouds and bright sun in the background

According to Lifecycle Insights’ Verification Management in Aerospace and Defense study, 56% of programs experience significant disruption to the schedule or cost weekly or more frequently. Findings from the same study show that 42% reduce program investments due to delays in the aircraft certification schedule. Many accept this as a way of life in the industry, but some companies execute programs far more efficiently, avoiding disruption and delivering on time.

Watch this webinar with Aviation Week to learn how to avoid issues that delay aircraft certification.

Common issues that delay aircraft certification

Because aircraft are such complex products, there are a number of issues that can derail aircraft certification and cause delays and cost increases. These include disjointed data systems, design changes, barriers with virtual testing, and the cost of building and maintaining physical test assets. Each of these issues is discussed thoroughly in the webinar.

Speed up aircraft certification

One way to speed up aircraft certification is to unite all program data in a single source of truth. Watch the webinar to learn more about how a single source of truth can help manage risk and avoid the issues listed above.

Topics covered in the webinar include:

  • Causes of costly delays in achieving compliance
  • How design changes impact your program schedule
  • What you can do to minimize schedule disruptions and late changes
  • Tips for ensuring an efficient approach to aircraft testing, verification and validation

Conoce a los ponentes

Siemens Digital Industries Software

Todd Tuthill

VP of Aerospace, Defense and Marine Industry

Todd joined Siemens after more than 30 years in the industry. Todd’s engineering background includes aerospace systems design, with several functional engineering and program leadership roles. His aerospace career spans McDonnell Douglas/Boeing, Moog, Raytheon and Siemens. He is a passionate advocate for advancing digital transformation across A&D and marine industries.

Lifecycle Insights

Chad Jackson

Analista y CEO

Dirige los programas de investigación y liderazgo intelectual de la empresa, da ponencias en eventos de la industria y analiza las soluciones tecnológicas emergentes. Su carrera de 25 años se ha centrado en mejorar la capacidad de los ejecutivos para obtener valor de las iniciativas de ingeniería basadas en tecnología durante la transición de la industria hacia productos conectados inteligentes.

Recursos relacionados