On-Demand-Webinar

NVIDIA: High-Level Synthesis in Agile System-on-Chip Flows: Overview and Techniques

Geschätzte Wiedergabezeit: 19 Minuten

Teilen

NVIDIA's introductory slide

Catapult High-Level Synthesis has been successfully employed within NVIDIA for multiple generations of system-on-chip research demonstrations. This talk provides a brief overview of NVIDIA Research’s use of Catapult HLS and highlights some useful features and flows of the Connections library, such as the ability to back-annotate SystemC simulations to identify and fix performance bugs.

Vorstellung des Referenten

NVIDIA Research

Nathaniel Pinckney

Senior Research Scientist

Nate Pinckney received his B.S. degree in engineering from Harvey Mudd College in 2008, and his Ph.D. in electrical engineering from the University of Michigan in 2015. He has authored or coauthored over 40 publications in the areas of high-level synthesis methodologies, low-power VLSI design, and cryptographic accelerators. In 2015, he joined NVIDIA in Austin, TX.

Verwandte Ressourcen

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification
Webinar

Infineon: HLS Formal Verification Flow Using Siemens Formal Verification

High-Level Synthesis (HLS) is design flow in which design intent is described at a higher level of abstraction such as SystemC/C++/Matlab/etc.

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis
Webinar

Infineon & Coseda: Facelifting a SystemC System Level Model Towards Physical Prototype – Adoption of High-Level-Synthesis

Infineon & Coseda present on the adoption of High-Level-Synthesis at an existing SystemC system level model.

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation
Webinar

CEA: Bridging the Gap Between Neural Network Exploration and Hardware Implementation

CEA presents a methodology that bridges the open-source DL framework N2D2 and Catapult HLS to help reducing the design process of hardware accelerators, making it possible to keep pace with new AI algorithms.

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?
Webinar

High-Level Synthesis & Advanced RTL Power Optimization – Are you still missing out?

Discover how C++ & SystemC/MatchLib HLS is more than just converting SystemC to RTL. In the RTL Design space, we will cover our technology for Power Optimization with PowerPro Designer & Optimizer.

Alibaba: Innovating Agile Hardware Development with Catapult HLS
Webinar

Alibaba: Innovating Agile Hardware Development with Catapult HLS

At the IP level, an ISP was created within a year using Catapult, a task impossible using traditional RTL. To reduce dependency on designer experience, Alibaba introduced an AI-assisted DSE tool.