On-Demand-Webinar

Drone noise reduction

Ensure urban air mobility technology adoption using simulation and test

Geschätzte Wiedergabezeit 49 Minuten

Teilen

A drone carrying a box and far-field simulation of the noise created by a stationary drone

Drone noise mitigation is a key enabler for urban air mobility technology adoption. Noise pollution is one of the main reasons why helicopter operations are often restricted. Thanks to the distributed electrical propulsion architecture, eVTOL air taxis and drones offer a perspective to reduce sound levels by 15dB at 500ft compared with helicopters.

Achieving this objective is critical to decreasing the overall journey time and thereby increasing the overall attractiveness of this new mobility mode. The challenge at hand is to design disc loading, rotor tip speed, propellor interactions and vehicle scattering in such a way that the overall in-situ noise levels are reduced.

It is a multidisciplinary issue, calling for the combined use of various simulation and testing techniques.

Drone noise

You will learn how to:

  • Combine CFD simulations and acoustic propagation together with raytracing methods to capture drone noise behavior at different scales
  • Model and validate noise sources against physical testing
  • Analyze propellor interactions influence on the noise signature
  • Understand how installation effects of the vehicle influence far-field noise levels
  • Gain insights into the effect of the urban environment on the noise

Drone noise analysis: von Karman Institute for Fluid Dynamics example

A numerical analysis carried out at the von Karman Institute for Fluid Dynamics will be presented dealing with drone tonal noise sources and their near- and far-field propagation patterns. Find out how to:

  • Validate the simulation methodology over a quadcopter against measurements available in the literature
  • Investigate the effects of the rotor-on-rotor interaction, and presence and absence of the body
  • Evaluate the sound scattering effects due to the presence of the drone body

Vorstellung der Referenten

von Karman Institute for Fluid Dynamics

Alessandro Zarri

Postdoctoral Researcher, Environmental and Applied Fluid Dynamics Department

Alessandro obtained his master's degree in 2017 from the faculty of aerospace engineering at Politecnico di Torino, Italy. In 2021, he received his PhD at the École Centrale de Lyon, France, with a research work based on aeroacoustics of automotive cooling fans carried out at the von Karman Institute for Fluid Dynamics, Belgium.

Siemens Digital Industries Software

Jens de Boer

Simcenter Solution Manager für die Luft- und Raumfahrt

Jens de Boer ist leidenschaftlicher Luft- und Raumfahrtingenieur. In den vergangenen 14 Jahren bei Siemens hat er mit Luft- und Raumfahrtunternehmen zusammengearbeitet, um deren Simulations- und Testprozesse während des gesamten Entwicklungszyklus anzupassen und zu optimieren.

Verwandte Ressourcen

Urban air mobility
Webinar

Urban air mobility

Empower advanced air mobility by adopting a digital twin approach, from early concept studies and design to verification and certification. Learn how.

Umfangreiche Lärmreduzierung bei Flugzeugen
White Paper

Umfangreiche Lärmreduzierung bei Flugzeugen

Minimieren Sie die Lärmbelastung durch Flugzeuge und verbessern Sie den Kabinenkomfort mit innovativen Konstruktionstechniken, um den Flugzeuglärm deutlich zu reduzieren.

Accelerate eVTOLs crashworthiness design with an integrated safety development approach
Webinar

Accelerate eVTOLs crashworthiness design with an integrated safety development approach

Improve urban air mobility safety performance by applying a fast system methodology