webinář na vyžádání

Introducing temperature and velocity dependent tyre modelling and its impact on vehicle dynamics

Sdílení

Introducing temperature and velocity dependent tyre modelling and its impact on vehicle dynamics

Tyres are a crucial component of the chassis and considerably influence the vehicle dynamics. To engineer for optimal vehicle performance, vehicle OEMs, chassis and vehicle integration departments are required to adapt tyre models to a broader range of operating conditions, balance performances and speed up the time-to-market.

Tyre performance is known to be highly dependent on the tyre thermal state and its forward velocity. Important passenger car tyre characteristics as the cornering stiffness and peak friction may vary up to as much as 20% as a function of Temperature &Velocity throughout their normal operating window.

With the introduction of the Temperature & Velocity model extension to its Pacejka’s Magic Formula based Simcenter Tyre products, Siemens offers Vehicle Dynamics engineers, Tyre testing and modelling experts the possibility to explicitly model the effects of temperature and velocity on the tyre performance. This further increases applicability and accuracy of the tyre model in vehicle simulations ranging from handling to durability.

Register to webinar to learn:

  • How the simulation fidelity can be increased for maneuvers throughout which the tyre temperature and/or velocity changes (e.g. ABS, ESC or laptime simulations)
  • How to manage tyre initial thermal state changes from one simulation to the other, for example to investigate the influence of seasonal conditions on vehicle performance
  • How the tyre testing protocol and model parameterization needs to be adapted for the Temperature & Velocity Tyre Model extension
  • How MF-Tyre/ MF-SWIFT users can benefit from the modular T&V extension both for Engineering Desktop & Real-Time applications

Tyre Simulation and Testing

Modelling tyre performance requires a lot of expertise and specialization. For this purpose, Simcenter offers engineers scalable and customized solutions through an end-to-end tyre modelling method that provides high accuracy, efficiency and tool standardization.

Introducing temperature and velocity dependent tyre modelling

Tyre performance is known to be highly dependent on the tyre thermal state and its forward velocity. In order to describe the impact of these effects on the vehicle dynamics, Siemens presented a scientific paper at the 2020 SAE World Congress: “A Study on the Effect of Tyre Temperature and Rolling Speed on the Vehicle Handling Response”.

A methodology for managing vehicle dynamics simulation for automated driving

This webinar outlines the vehicle dynamics simulation requirements in the context of autonomous driving.

Tyre Model Marketplace

Easily access high-quality tyre model parameter sets for vehicle dynamic simulations



Speakers

Seznamte se s přednášejícími

Siemens Digital Industries Software

Hans Van Den Wijngaert

EMEA Portfolio Developer Automated Driving, Occupant Safety & Tyre Simulation

Siemens Digital Industries Software

Willem Versteden

Product manager Simcenter Tyre